4/3/2017 10:46 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Is this error solved? I faced this error too. Below Text retrieved from OS compilation log. BAVN17403/1.FbkCloseOut#Value already exists BAVS17001/1.Ctrl#Value BAVS17001/1.Ctrl#Value already exists BAVS17002/1.Ctrl#Value BAVS17002/1.Ctrl#Value already exists *** Error(s) ***: Internal error: The compilation of archive tags was canceled. Error number: 16003 An error occurred while updating the archive tags. PCS7V 8.2. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/3/2017 1:20 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
My problem was solved. The error was caused by my AS project. I retrieved a compiled AS project (previously compiled in local station) and dump it into master engineering station for OS compilation. I solved the issue with a full compilation on AS project using the engineering station and later recompile the OS again. Thanks. 20210919 update - PCS 7 V9.0 SP3 Error:: Internal error: The compilation of archive tags was canceled. Error number : 16003 An error occurred while updating the archive tags. Error message 2: Compile OS (302:3061) An error occurred while updating the archive tags. Unknown error (might be related) : Updating the WinCC data. ***Warning***: The group display hierarchy could not be created. The method ICCCSigGdo->ConstructCSigHierarchy returns error code - 2147467259 Possible root cause (My thought) : 1. Improper shutdown during OS compilation 2. multi AS user projects were compiled or improper managed in other engineering workstations (multi-engineers). (Software version might not be exactly the same) Resolution: 1. study OS compilation log , Find "error". 2. identify the last tag number that cause the stopped. 3. identify which PLC/AS project it located at. 4. Full Compile that AS project with generate Module driver. 5. redo OS compilation again and see issue resolved. My real step on 20210919 - during office development (If this issue occurred at site, the below steps are last resort. MUST seek client appproval and understand all the consequences before execution) 1. Backup multiproject 2. delete and remove multiproject 3. restore previous day multiproject that were working fine for OS compilation and download. 4. open the OS wincc application 5. go to alarm logging and tag logging , reset 6. close the OS wincc application 7. go to the affected AS project 8. clean up chart and block database 9. check the block properties in component view of the S7 program on the AS project 10. get fill level to check the reorganize needed 11. reorganize the AS user project to bring down the block fill level. (DO NOT do it on OS user project) 12. Full AS compilation with generate module driver 13. Full OS compilation with memory reset. 14. Issue resolved.
|
Last edited by: JazTai at: 09/19/2021 13:42:33Last edited by: JazTai at: 09/19/2021 13:53:41Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
4/3/2017 2:39 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
I also had such an issue.. I compiled the OS (full+memory reset) through ISO protocol instead of named connections. Tags are being created new on ISO protocol and deleted on named connections. Then I recompiled again to the named connections and then all was good. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
4/13/2017 5:15 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
May i know more details on the archive configuration tool? Im interested on this. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/15/2017 10:38 AM | |
Joined: 6/23/2008 Last visit: 4/22/2024 Posts: 1165 Rating: (279)
|
Hi JazTai, it is a tool wich works with excel. You can create/edit/delete archives of your WinCC project in excel. It works by import/export between excel and your WinCC project. As your archives in PCS7 are usally created by OS compilation, it is not very intresting for PCS7. From a certain version of PCS7 on, you won't find it on the PCS7 setup DVDs anymore. You need a setup DVD of the corresponding WinCC version to install it. And from WinCC 7.3 it's not available anymore at all (the same for 'WinCC Configuration Tool'). Anyhow, if you like to know more details see the document from this link and have a look to chapter 1.9. Best regards, mark |
Last edited by: mark1507 at: 4/16/2017 6:02:26 PM"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
This contribution was helpful to1 thankful Users |
4/17/2017 12:24 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Thank you so much. i will take a look at the document. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on