5/19/2010 7:10 AM | |
Posts: 288 Rating: (22) |
Dear all, We have upgraded 8 SIMATIC 547B Industrial PC’s with PCS7 V7.0 SP1 to PCS7 V7.1 SP1. For doing this we executed the setup disc of V7.1 SP1 on all the machines and chose to update the existing installations. The installations executed without problems.We are trying to set up a server client system on 6 of these PC’s in the following configuration: Ø 1-ES Ø 2-OS Servers (Redundant) Ø 3-Clients After starting a new project, we were able to configure all the PC stations from the ES as well as transfer the project to the OS servers. However, when we tried to compile the OS project in the ES, we are getting errors. The screen shots are attached herewith. In addition, the OS project editor could not be called up individually from the WinCC explorer. The redundancy settings were also not accessible in the same sense. Please suggest a method of solving these problems. AttachmentERROR BASKET.zip (85 Downloads) |
Follow us on