7/7/2017 10:18 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi Duccio, Do you have more info? PCS7 version, do you get an error code when starting compile? Does the error logs show something? you can upload them if you want--> C:\Program Files(x86)/SIEMENS/WinCC/diagnose How do you transfer the multiproject? Archiving project on es1 and retrieve on es2? or another way-> Multiproject engineering? |
If I could help you, you can use the RATE button. Thank you. |
|
7/7/2017 11:17 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, The easiest thing to check is that your example project (installed by default): APL_Example_EU does start and complete it's OS compilation. If not, it means something is wrong with the installation/VMware. Steps you can take: 1. Close all Siemens applications and execute Start->and type: reset_wincc.vbs. Wait for the popup, press OK and restart the VMware. 2. The OS compiler is started by process: "s7uvmapx.exe". Copy this file from the other VM to your VM. 3. If this not helps, reinstall: AS-OS Engineering from the PCS7 DVD. Otherwise use a copy of your colleague's VMware? |
Last edited by: Oreca at: 7/7/2017 11:29:07 AMLast edited by: Oreca at: 7/7/2017 11:33:09 AMLast edited by: Oreca at: 7/7/2017 11:36:11 AMIf I could help you, you can use the RATE button. Thank you. |
|
7/7/2017 1:54 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
OK, seems multiproject related... You can try to create a new archive on the working vm and retrieve on your vm. Maybe something went wrong with archiving....I hope, |
If I could help you, you can use the RATE button. Thank you. |
|
7/7/2017 2:41 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Yes, let me know! |
If I could help you, you can use the RATE button. Thank you. |
|
9/10/2021 6:40 PM | |
Joined: 12/7/2011 Last visit: 4/3/2024 Posts: 382 Rating: (9) |
I, mi sorry but at that time i moved on into another project. so i dont know which was the solution. |
Follow us on