1/26/2010 6:04 PM | |
Joined: 11/15/2009 Last visit: 8/16/2024 Posts: 380 Rating: (47) |
Can you for test on OS PC in WinCC Explorer a new projekt create (and delete)? Is it basically possible? Regards |
2/1/2010 3:55 PM | |
Joined: 12/23/2008 Last visit: 5/31/2022 Posts: 40 Rating: (0) |
I'm using PCS7 v 7.0 SP3/WinCC 6.2 SP3 |
7/15/2010 9:08 AM | |
Posts: 691 Rating: (37) |
Hey Load log Source: D:\Prog\BATT_MP\BATT_PRJ\wincproj\CL2\winccom\ Display load log... 7/15/2010 11:08:54 AM : The project was locked. |
7/15/2010 12:52 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi, have you Already Downloaded the Client WinCC Configuration ? way you want to download the WinCC Project again? Client WinCC configuration Does not Containt any .PDL, it will fatch from the Server Very time. Delete the WinCC Folder on the D:\Prog\BATT_MP\BATT_PRJ\wincproj\CL2\winccom\ & try to Download the Configuration Again. |
Ammy |
|
Follow us on