5/11/2016 12:34 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
hello, I have an S7-300 CPU 315-2DP and I have a problem with the outputs, you can even in the two attached example does not work with the A4, A5, A6 ... but works with A0, A1, A2 and A3, if you have a solution I will be grateful
Attachmentexp2.pdf (182 Downloads) |
Last edited by: kam3216 at: 5/11/2016 12:36:44 PMLast edited by: kam3216 at: 5/11/2016 12:43:28 PM |
|
5/11/2016 12:48 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
I have nothing in my programe that the two lines quoted attached |
5/11/2016 1:07 PM | |
Joined: 8/31/2013 Last visit: 4/18/2024 Posts: 606 Rating: (41) |
Hello Did you compare your program with the online program which is downloaded in the PLC |
Warm Regards |
|
5/11/2016 2:17 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
yes it is the same programe but what is surprising is that it works well with A0.0 to A3.7 .... and not with A4.0 ..... |
5/12/2016 3:07 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
with real output Led on output card |
5/12/2016 4:30 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
hi |
5/12/2016 8:06 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
This is already done if I change the address of his works but only with address 0,1,2 and 3 |
5/13/2016 10:58 AM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
how to do a procedure if possible |
Follow us on