5/13/2016 1:14 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
I'll do the verification and answer you |
5/13/2016 3:13 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
if there is another solution proposed for that I try to do so on Sunday |
5/15/2016 1:48 PM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
Here is my config, I compared with two other cpu and it is the same. |
5/15/2016 5:16 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
And if you post your project to us? |
5/16/2016 9:24 AM | |
Joined: 12/13/2015 Last visit: 4/1/2024 Posts: 22 Rating: (0) |
have a simple project and published the top |
5/16/2016 11:12 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839)
|
As per your attached picture, you told that when you program output with address A4.x it works with HW config. A0.x to A3.x It's very strange!! Did you have any call in OB1 for any other FC. Did you downloaded any FC in the OB1? To be sure of that please reset the contents of MMC How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)? |
Ayman Elotaify |
|
Follow us on