4/16/2018 7:13 PM | |
Joined: 11/11/2017 Last visit: 9/23/2024 Posts: 189 Rating: (4) |
can someone take a look at this program for me and offer some advice. i am really struggling on this one and i need some guidance. the oven is controlled by a set point which is a user variable entered on the TDE so it wont be the same set point all the time but i need it to turn a timer when the temperature is reached for example: temperature = 100c set point = 150c when temperature = 150c it will enable a output to say the oven is at temperature and a count down timer can now be activated by a input when time as elapsed a output will come on but after the time as elapsed the timer can be started again so long as the temperature is at set point (this case 150c) in summary the timer can ONLY be activated when the temperature as reached set point. like i said i am really struggling to make this work so a little guidance would be a great help. thanks AttachmentOVEN non bleed fan r1.zip (140 Downloads) |
Last edited by: thedodgy1 at: 4/17/2018 12:27:31 PMLast edited by: thedodgy1 at: 4/17/2018 12:28:15 PM |
|
4/17/2018 3:38 PM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33833 Rating: (4205)
|
Like this?
AttachmentCompare_setpoint_actual_FS4.zip (161 Downloads) |
Follow us on