8/21/2013 9:34 AM | |
Posts: 113 Rating: (22) |
Have you gone online and watched the operation of the line, I usually find it is something obvious rather than a PLC error. |
8/22/2013 6:31 AM | |
Posts: 461 Rating: (29) |
In s7 200 networks u havent usd the pos trigger... For pos triggering the bit m8.6, u have to use the pos edge indtruction . C the img |
8/22/2013 7:26 AM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
@Nelliyan randy Yeah thats the issue with 200. The logic working only without P trigger.
|
"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
This contribution was helpful to1 thankful Users |
Follow us on