Industry Online Support
Technical Forum
12/28/2019 6:06 PM | |
Joined: 6/28/2011 Last visit: 4/24/2024 Posts: 6 Rating: (0) |
Hello sir The P1512 parameter (Additional torque 1 scaling) of d425 firmware V5.3 cannot be modified, but V5.2 can be modified (100%). After the original program upgrades the hardware to V5.3, P1512 cannot be saved after compilation. I follow As shown in the screenshot below, why? [snip] |
Last edited by: Jen_Moderator at: 12/30/2019 10:29:36Removed link and added file as an attachment. |
|
Follow us on