9/19/2017 5:54 PM | |
Posts: 31 Rating: (0) |
I need to replace a P350 (6AU1350-3AK41-1BE2). I have the exact same new unit and a ghost from my old P350. When I start the new P350 with the ghost, Windows boot, Protools RT and Simotion start, then a message appear "Updating Hardware Configuration" and few seconds after that P350 freeze forever. I must turn off power to be able to reboot, and after this "power off reboot" I got error, blue screen, real mess. I finally be able to login with windows safe mode and check the event viewer (see picture). Actually I can't run with my new P350, do I miss something? Can we run ghost on a spare unit or we need to reconfigure hardware (CCAgent look for MAC)? Attachmentpicture.zip (113 Downloads) |