8/25/2014 8:38 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306)
|
Hello Alex_o_Lobo Normaly such problems would be caused by improper installation / configuration of the profibus network. In case you can provide more details regarding : a) What was the original Profibus Network Configuration ? b) Where and how many PAC meters were added in the network ? c) Speed and Length of Original and modified network d) No of nodes in the Original and modified network. PAC 3200 can be operated on DPV0 as well as DPV1 ( Though I am not convinced that Using DPV1 GSD files is the cause of the problem. ) You can download the PAC 3200 GSD File for DPV0 from this page : GSD files for PAC3200 Manual for PAC PROFIBUS Module Hope this helps Cheers Navnag |
Last edited by: Navnag at: 8/26/2014 7:04 AMLast edited by: Navnag at: 8/25/2014 8:42 PMManual Link Added There is no such thing as the last bug in a program |
|
8/26/2014 6:07 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Alex_o_Lobo GSD files for V1 are available for both the version of PAC3200 7KM9300-0AB00-0AA0 : DPV1 / DPV 0 7KM9300-0AB01-0AA0 V4.0: DPV1 Only It is also possible to Upgradeot Downgrade the Firmware versions , See : Delivery release: Expansion Module PROFIBUS DPV1 However as manmeet has pointed out, the DPV1 files also behave as DPV0 when used in a profibus network which does not support DPV1 ( e.g. downstream of a Y-Link ) However haing said this, I still believe that the source of problem may not be the GSD files, but network configuration. Details of the system configuration, may help understand the issue better. Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
8/26/2014 6:40 PM | |
Joined: 7/8/2013 Last visit: 7/20/2016 Posts: 3 Rating: (0) |
manmeet We will check on the field |
Follow us on