6/10/2009 7:17 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
i try to translate this. hope it is correct: |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
6/10/2009 8:49 AM | |
Posts: 217 Rating: (52) |
Hi, If I understand your problem correct. You need to connect an encoder to a motor and get the pulses to s7 200 and you want to control it using a HMI (by entering values). I think you can use HSC or normal counter (depending on the speed) to count pulses of the encoder. Then you can control the motor using your HMI (probably comparing values). Also see the manual and the help of microwin software under HSC and sample programs under tips in you microwin documentation. |
6/10/2009 11:47 AM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Thank you Sabine, the translation was not bad at all. Paul; To read an encoder value in a S7-200, start bystudying the HSC (high-speed counter)instructions in the Microwin Online help and in the S7-200 System Manual. http://support.automation.siemens.com/WW/view/en/1109582 Unfortunately it does not seem to be available in Portuguese, maybe the Spanish version can help? You could also look at the FAQ at this link: http://support.automation.siemens.com/WW/view/en/2123175. Paul; Iso e um foro que usa Ingles, o Alemaocomo idioma. As repostas seran em Ingles, geralmente. A gente aqui pode ajudar, e querem ajudar-o, mais voce precisa fazer um esforzo dissa manera. Voce pode escreber ao Sr. Denilson Pegaia, quem trabalha com Siemens em Brazil, pode ser que ele pode ajudar mais (tambem ele e experto em S7-200nesse foro): atencao.cliente.ac.br@siemens.com As instrucoes pra ler os pulsosde um "encoder" sao grupados baixo o nomem "HSC" (High-speed counter); veja a ajuda de Microwin, e o manual sugerido arriba. Com amistad, e faiz favor de perdonar os errores em Portugues, preciso praticar mais, muito mais. Daniel Chartier |
Follow us on