12/16/2015 9:16 PM | |
Posts: 111 Rating: (1) |
I need Force guided contacts cubical relay in SIEMENS. Can anyone provide me the part numbers. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/17/2015 2:40:48 PMNew subject after splitting |
|
12/17/2015 2:01 PM | |
Posts: 111 Rating: (1) |
Can anybody tell me the part number of siemen cubical relay with safe guided contacts as I am unable to find it. |
12/17/2015 3:42 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Shahjee, Which model? Safety Systems - Industrial Controls - Siemens |
This contribution was helpful to1 thankful Users |
12/17/2015 5:03 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Shahjee; If you accept the definition below (taken from this site : http://www.jconsultingonline.com/safety_stop_circuits_and_master%20control%20circuits.htm): Force Guided Contacts - Force guided relays, also known as directly driven relays or positively driven relays, have contacts that are mechanically linked. This mechanical link for the force guided contacts provides "monitoring" functionality that's not available in standard relays (non-force guided) in regards to the ability of the normally closed contact providing status for the normally open contacts.
Then you can have a look at this Siemens catalog extract and start your search: http://cmsapps.sea.siemens.com/controls/icc2010/10IndControl_%20pdfs/10IC_02/02_018.pdf
The complete catalog is available here, in sections: See section 2 for your application needs. Hope this helps, Daniel Chartier
|
This contribution was helpful to2 thankful Users |
Follow us on