Industry Online Support
Technical Forum
10/30/2014 8:39 AM | |
Posts: 1299 Rating: (136)
|
Hello, Can you please try to explain your issue again, maybe also with some screenshots? Maybe this link can help you: http://support.automation.siemens.com/WW/view/en/57025748 K!ke |
1/9/2015 8:53 PM | |
Posts: 4 Rating: (0) |
K!ke, We have around 2000 tags that we have set to 'cycle continous' this is really affecting the performance and respond time of our project as you can imagine. The tags do not need to be to scanned continuously however I am having an issue figuring out the best way to use 'On Demand' aquisition mode for these tags. I could use the UpdateTag event function however it is limited because there are only 100 different Update ID's (1-100) with each Update ID only able to be assigned to a single tag. Do you have a way to use 'On Demand' rather that continous cycling, I think there is a way to use arrays, but I haven't quite figured it out. Regards, Roman
AttachmentDoc1.pdf (255 Downloads) |
Follow us on