Industry Online Support
Technical Forum
6/13/2014 8:38 AM | |
Posts: 1368 Rating: (126) |
Hello walock, is it possible to post a thumbsketch of your configuration? The PNIO_RCV must be used, if the CP is in PROFNET IO mode. But your CP is not PROFINET compatible. Do you really need the CP? The CPU also have a PB interface....and a PN-interface Look here https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=29548878731&Language=en-US&TopicId=28244371595 Greetings |
6/19/2014 12:51 PM | |
Posts: 24 Rating: (0) |
Hi I will try to do that. Have updated the information. The CPU has 2 PN interfaces so it can connect to the PN IO. |
Follow us on