3/21/2012 5:28 AM | |
Posts: 6 Rating:
|
Hi all, I have installed PC Access sp4.IP of PLC: 192.168.0.1. My PC: 192.168.0.2 I don't know TSAP (Local and Remote). I read on Manual PC Access, and I set Local, Remote. You can help me about this problem. I have watched:/tf/WW/en/Posts/49561, I do the same web page but still error report. Thank friends. |
3/21/2012 9:39 AM | |
Posts: 2930 Rating:
|
Hi, see the instruction how to install the PCA SP in this FAQ: http://support.automation.siemens.com/WW/view/en/58495870 If you wnat toupdate PCA SP6 on a PC with Win7 or XP SP3 operating system, then you need the original PCA installation CD-ROM, or PC-Access installed on the PC with supported operation instruction. In this case you have to zip the named file (on the Pc with supported operating system), copy the zippend file to the PC with the new operating system. Her unzip the file and then start the installation. If you have the original PCA Installation CD-ROM then you can enter it during installation. If this doesn't help and you have tried to update without folloing the installation instruction in the FAQ (or you have used the PCA SP4 installation DC-ROM on your PC with XP SP3 or Win7), then you may need to clear you PC manually. Search for "installation" in the FAQ's for PC Access. Hope this helps |
Follow us on