Industry Online Support
Technical Forum
9/8/2011 3:15 PM | |
Posts: 69 Rating: (3) |
Dear experts, Iam also facing same problem .I install Step7-v5.5 completely and then i open set pg/pc.I select pc adapter mpi and then click properties.After pressing properties it shows local connection not available.That is ok.But it didn't show the port details in the set pg/pc screen.Kindly find the attched copy and give the remedy.My major doubt is if i connect in online it will work or not. R.R
Attachmentproblem in driver installation for the pc adapter.zip (67 Downloads) |
Last edited by: Blue Moderator at: 09.09.2011 13:20splitted from /tf/WW/en/Posts/48165#top and renamed |
|
9/9/2011 4:48 PM | |
Posts: 376 Rating: (57) |
Hello R&R, What versionof Windows operating system have you installed? What version of STEP 7 have you installed? Do you use an PC or PG ( example Siemens PG)? Please reads the following information. Possible you still find a note. http://support.automation.siemens.com/WW/view/en/44914248 Best Regards Azteke0110 |
5/13/2014 10:34 AM | |
Posts: 65 Rating: (5) |
From your attachment it seems that you are using Windows 7 and i think that pc-adaptor v2.0 driver is not compatible with windows 7 u can check thae link below
|
Follow us on