5/3/2008 3:57 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello webpower; In the PC Adapter USB hardware manualthey show you the connection diagram you can use for your purposes. But they also propose a recommended power supply and add a caution: Supplies (not included in the PC Adapter USB) To operate the PC Adapter USB to MPI/DP interfaces which do not have a 24V supply voltage, you can order an external power supply (order number: 6ES7 972-0CA00-0XA0). Caution Always connect the PC Adapter USB to power supplies with limited power or NEC Class 2. |
Follow us on