Industry Online Support
Technical Forum
10/22/2010 11:38 AM | |
Posts: 1 Rating: (0) |
Will convert a file can be converted to a file% PCP => .S5D understand Step5 |
10/22/2010 3:39 PM | |
Joined: 10/7/2005 Last visit: 3/28/2024 Posts: 3002 Rating: (1045)
|
Hello frank11 I presume you have a PCP/M operating system based S5 file an need to convert it to a MS DOSbased S5 file to be able to open it with a DOS or Windows based version of Step 5, correct? If so, you need to convert the file using PTools which you can download from HERE. Note that PTools is also still part of Step 5 and can be found under the File menu (and its usage is explained in the Step 5 manual), you are however blocked from using it if your OS is newer than Windows 95 (see HERE for more). I hope this helps and answers your question, but if not please explain in some more detail what you are trying to do. |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on