Industry Online Support
Technical Forum
7/9/2012 9:49 AM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Хай богдан_a_1976 , the problem is that you can not use Smart Object of type Status Display for linking some bit of a Word (only in case of block icon). You can use only Status Display (extended): - put a new Status Display (extended) object to your block icon; - open Configuration Dialog; - deactivate option Use group value for display; - in the bit selection area select "from status word4" (it's just for example, cause you can select "..word1" as well) and right here assign a bit of a word; - the other three fields should contain "no status word"; - assign pictures; - now finish editing and add a property "Status4" in the Configuration Dialog with assigning to it your StatusDisplay object and it's property "StatusDisplayName.Status4"; Now look at my modification of a MotL block icon. I'm using UserStatus (bit 0) input of a MotL block to display additional digital value. Attachment@PCS7Typicals.zip (245 Downloads) |
7/10/2012 12:19 PM | |
Posts: 27 Rating: (0) |
Thanks a lot! It worked. |
Follow us on