6/26/2015 12:31 PM | |
Posts: 1 Rating: (0) |
Dear All I’m using AS 410 H and PCS 7 -V8.0 DCS which will be communicating with devices over parallel redundant Profibus-DP communication protocol. On profibus segment I have two different device manufacturer Biffi ICON2000v4 and BERNARD Intellis. All the devices are pofibus slave redundant. I installed both GSD of field devices ant tried to configure them. But I have different behaviour between two devices type. BERNARD will be automatically connected on both Profibus networks. But BIFFI device will allow a connection only to one Profibus network (like a simple device). You can see the screenshot attached. I checked both GSD file content and did not find big differences about redundancy. Both devices have “Redundancy=1”. Biffi is “GSD revision=4” and Bernard is “GSD revision=5”. Attached to this topic You can find both GSD. Can someone tell me why GSD of Biffi Device will not allow me to manage the redundancy? Thank You Fabio AttachmentMyattach.zip (54 Downloads) |
Follow us on