12/7/2015 11:03 AM | |
Posts: 42 Rating: (3) |
Hi experts, I am working with PCS 7 V8.0 SP1, I have issue to link up those "Area buttons" in winCC Runtime. From the OS Project Editor, under <Area> tap, when I click the "Preview", I am able to see the "Flammable Gas Room" which I have assigned to one of the area button. But when I go to runtime, it shows <no text> in that button, and the button has no function. May I know what could be the problem? Thank you very much! Sytupit Attachmentpcs7_Area_error.zip (266 Downloads) |
Last edited by: Sytupit at: 12/7/2015 11:22:45 AM |
|
12/14/2015 6:59 AM | |
Posts: 42 Rating: (3) |
Hi schufri, I checked the text library. I can see those container name in the text library. They are the same. Thanks. Best regards, Sytupit |
Follow us on