Industry Online Support
Technical Forum
9/10/2012 1:22 PM | |
Posts: 26 Rating: (0) |
Dear All, Is it possible to communicate PCS 7 V8.0 with CPU 412-2DP, or how to use PCS 7 with CPU 412-2DP Any help is highly appreciated. |
9/12/2012 4:40 PM | |
Posts: 836 Rating: (99)
|
Hi, what exactly do you want to do? You can use the 412 in HW config by using not the "PCS 7", but the "Standard"filter in the HW catalog. But you won't be able to use all PCS 7 featured blocks, because the AS is not supporting everything. Note, that this is not PCS 7 conform. Maybe you have a look at this application. It described how to integrate S7300 and Panles into PCS 7 environment. MAybe you can get some ideas from it: http://support.automation.siemens.com/WW/view/de/50708061 |
Follow us on