8/3/2015 9:15 AM | |
Posts: 19 Rating: (0) |
Hi everyone, What would be the reason if the APL_Trend is not responding if it is set in archive tag connection? Hope you could help me. |
8/3/2015 9:51 AM | |
Posts: 19 Rating: (0) |
Is this something to do with Global C-Script? |
8/6/2015 8:01 AM | |
Posts: 19 Rating: (0) |
ToMolthoff:
Is it available as Archive trend? Can you browse it if you make a manual trend (from the trend system in the bottom button bar? If not: Select the archive option in CFC at the IO. Sometimes it helps to switch between longtime and archive (make sure you compile the OS between switching). I'm not sure if you are missing a server prefix... I've got Servername::Systemarchive\Tag.IO Hope you can solve it, please let us know Thanks for the response. Yeah, it is available as archive trend. If I make a manual trend from wincc the archive tag is working, but in the APL faceplate trend (PCS 7 faceplate) the archive tag is not working. I can't see the archive option in CFC at the IO (Can you please show me where it is?). I'll try to check the global c-script where it call or set the archive/tag name. Then If I solve it I'll tell it you. Thanks again :) |
Follow us on