1/23/2015 11:05 AM | |
Joined: 1/10/2011 Last visit: 1/11/2023 Posts: 10 Rating: (0) |
Hi, I need help with the following problem in PCS7 7.1 SP1 I have created a PCS7 project in ES with AS OS Server and OS Client PC and downloaded to AS OS server PC and OS client PC. OS Server is working fine. Bus there is a problem with OS CLIENT.It is showing screen navigation buttons active and server status OK, but Screen are not getting opened by pressing the buttons. I have attached a pdf file showing both Server and Client screen for your referance. Regards, Swati
AttachmentPCS7pic.pdf (415 Downloads) |
Last edited by: swatipatwardhan at: 1/23/2015 11:06 AM |
|
1/24/2015 4:46 PM | |
Joined: 12/22/2014 Last visit: 10/7/2021 Posts: 173 Rating: (23) |
Hello swatipatwardhan There is a button in the lower button bar which you can use to performa manual selection of the picture. Does this succeed? |
Greetings |
|
1/24/2015 11:06 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Swati, Can you open the apdiag.exe tool during runtime and press on: output window and then try to open the picture on the client. It should output an error, please emclose this in your post. You can find the toolbar button: tools on the second buttonset in the lower screen. You can also open the tool under: c:\program files\siemens\wincc\utools\apdiag.exe Thanks! I can tell you more when I know what the error line is. |
If I could help you, you can use the RATE button. Thank you. |
|
1/27/2015 5:23 AM | |
Joined: 1/10/2011 Last visit: 1/11/2023 Posts: 10 Rating: (0) |
Hi Jaime Enrique, All PC stations have same(ES,Server and Client) user id and password. Thank you, Swati |
1/28/2015 8:27 AM | |
Joined: 1/10/2011 Last visit: 1/11/2023 Posts: 10 Rating: (0) |
Hi Oreca, I am attaching here the screenhshot showing error msg the as per your suggestion.Kindly go through it.I am still facing the same problem.I can not open screen in Client PC. Msg Inside the window(apdiag.exe) is as follows: SSMRTChangeWorkField failed: Split Screen Manager: Invalid Picturename. OnClick: SSMGetSAPictureAndObjectNameEx failed Pic = , Obj = Thank You, Swati Attachmentc1.pdf (283 Downloads) |
Last edited by: swatipatwardhan at: 1/28/2015 8:31 AM |
|
1/28/2015 9:00 AM | |
Joined: 12/22/2014 Last visit: 10/7/2021 Posts: 173 Rating: (23) |
Hello swatipatwardhan Can you check in the Simatic Managerthe OS Server assignment of the OS Client? Richt click on the OS Client WinCC project. Often the link to the OS Server is broken and you see a red line. You have to deselect and select the OS Server again. |
Greetings |
|
1/29/2015 5:25 PM | |
Posts: 1 Rating: (0) |
Hi, just for knowledge and for something similar that happened to me before, try from your client in a PC explorer windows address: \\ServerNameOS (put the hostname of your server after doble inverter slash \\) and check that you can enter until the folder Gracs, try to create a blank Notepad .txt file, if you have problems with that the problem is with some configuration or permissionwith share folders in windows. |
Follow us on