Industry Online Support
Technical Forum
11/13/2008 11:23 PM | |
Joined: 9/27/2007 Last visit: 4/11/2024 Posts: 37 Rating: (0) |
Dear's, I have a project with pcs7 v7 and cpu 414h.in this plant exist a dcs system with redundant abb freelance "AC800FR" in exist dcs some needed tag transfer to Citect HMI with OPCserver of freelance in ethernet bus. I want yo use cpu 414h with pcs7 v7 in other section of this depertment and so I want use pcs7 Instead Of citect in exist system that mean: " I must have one type HMI system for 414h and ac400f" 1-I want to know can i export FreelanceOPCserver tag's into wincc with OPC Channel into wincc server and delete citect HMI or not? 2-some data must to transfer from abb to siemens cpu for some logic's how can i do this? i attach configuration in pdf file please tell me your solution as soon as possible thanks with best regards rasool alizadeh AttachmentConfig.pdf (146 Downloads) |
11/15/2008 9:45 AM | |
Joined: 9/27/2007 Last visit: 4/11/2024 Posts: 37 Rating: (0) |
Protocal such as profibus or ethernet is approved from client |
Follow us on