4/23/2015 10:26 AM | |
Posts: 46 Rating: (3) |
Hi, which version of STEP 7 do you have? |
6/23/2015 8:51 AM | |
Posts: 11 Rating: (0) |
hello dear we use step 7 v 5.5 . best regards a.seyedzadeh |
6/25/2015 12:03 PM | |
Joined: 6/14/2006 Last visit: 4/29/2024 Posts: 301 Rating: (60) |
Please check https://support.industry.siemens.com/cs/document/28739248 if the modules you use are released for PCS 7 7.0. |
6/25/2015 1:12 PM | |
Posts: 567 Rating: (106) |
Please check also if the catalog profile in HW Config is a PCS 7 profile and not "Standard" and then insert the module. |
6/28/2015 5:29 AM | |
Posts: 11 Rating: (0) |
Dear Ralfinio We select all module from standard because in pcs7 v7.0 sp3 we do not have pcs7 catalog. |
6/29/2015 9:41 AM | |
Posts: 567 Rating: (106) |
Hi, based on your screenshot you have installed PCS 7 V7.0 SP2 and STEP 7 V5.5. STEP 7 V5.5 is not released PCS 7 V7.0 SPx!!! Maybe this is the reason why you don't have a PCS 7 catalog. But in a PCS 7 environment it is very important to use only released software!!! Which STEP 7 versions are released for PCS 7 V7.0 you can find under the following link: https://support.industry.siemens.com/cs/ww/en/view/64847781
|
Follow us on