1/23/2015 1:01 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
Hello guys, During my batch training, own project and example project (kitchen), the EOP haven't been used. Only the EPH. Can somebodygive me an example on when to use an EOP?? (SFC type). And that I can see the difference with an EPH? The manual is not clear about this, it says an EOP hasthe logic inside the AS, more then in a recipe and an EPH has the logicin a recipe and not so much in the AS. Thxx |
If I could help you, you can use the RATE button. Thank you. |
|
1/24/2015 6:19 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
Hello Jules, fellow dutchman;) That is what Siemens invented AS based batch for, to have the control recipe in the AS, rather on the batch server (PC based).. I want to know when you (must) use an EOP. What benefits has it over a EPH? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on