10/15/2012 6:47 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hello, I got the exam for pcs7 next week and I would like to know which questions you guys remember...I saw the tests on the sitrain page and the questions I got were difficult as I don't really know how to learn for this.... So If someone remembers a question they got on their exam, please share |
If I could help you, you can use the RATE button. Thank you. |
|
10/18/2012 10:19 AM | |
Joined: 10/26/2011 Last visit: 4/18/2024 Posts: 760 Rating: (190)
|
Hello Orega, |
Last edited by: Thunderstorm at: 10/18/2012 10:19 AMSIMATIC PCS 7 - Overview |
|
10/19/2012 6:20 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hello, It is an exam for PCS7. You can take the course, however this is a system course and not interesting because it is too basic. There are however multiple choice questions with more than one answer possible. A few examples taken from Sitrain test for PCS7: What voltage(s) can be deliverd by the power supply modules: answer: 5vdc or 24vdc. Which operating system is possible in a OS server in PCS7 7.1? A: XP3 and Windows 2003 server. What can be monitored with lifebeat monitoring? A: As failure+Failure of OS client+Failure of neighbouring OS server thus you have to select A+B+C So, If somebody has more??? :)
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on