5/14/2020 6:44 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, My French is not so good, like not at all, but it looks like your are using the dig_device library, but the blocks are missing/cannot be compiled. Dig_device sounds like an old library. You have to tell us a bit more. Is this project migrated? Was it working previously? Are you working on another ES? |
If I could help you, you can use the RATE button. Thank you. |
|
5/15/2020 6:58 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Hicham_hard is split to a separate thread with the subject Erroneous characters in the name of the facplate. Best regards |
5/15/2020 7:45 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
If you compile the project on another ES (for example, your own laptop), you have to have this library installed as well on that laptop. You can compile if you do not check Generate Module Drivers option under compiling settings. Also check if the library is still released for V9.0. I have heard of it, but never used it. There are a few manuals which let you update with or without new functions. Maybe this is a good source to look at. Migrating is not so easy, you have to do this in steps: V7.0-V7.1-V8.0 etc. Software update without new functions Software update with new functions |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on