8/19/2019 10:53 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear AutoGen_4972445, Yea, it means the s7connection was disconnected for xx seconds. What is your system architecture? OS Server-standby? or OS single? 1. Did you separate the network to terminal bus and plant bus? 2. can you check the diagnose file see any good diagnose info for troubleshooting? See attached. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/19/2019 3:49 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Try switching the Master to the other server to check whether there is the same issue or not ? This is to eliminate the possibilities on the CP card. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/19/2019 4:08 PM | |
Posts: 6 Rating: (0) |
There are no CP cards used in the Project. I've switched the OS Server's & it's not working out properly! Regards KK |
8/20/2019 2:45 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
So normal ethernet card is used, and you used IE S7 to connect AS-OS connection. What PCS 7 version are you using? Could you check the installed software in ES and OS Servers, see any available update on the software or not? And do you have any finding in Diagnose file? you can upload it. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on