5/8/2008 4:33 AM | |
Posts: 2661 Rating: (279) |
amk: |
5/8/2008 9:26 PM | |
Posts: 2661 Rating: (279) |
Yes, that's right. An OS Single station.
An OS single station license. The limitation is, there will be only 1 station. if it fails, the operator loses control. But you can always use the ES (with WinCC client RT license) as a standby for such emergencies. Also please check the following FAQ: What hardware and software do I need in order to work with CEMAT V6.1? http://support.automation.siemens.com/WW/view/en/21853589 Regards |
5/10/2008 10:25 AM | |
Joined: 6/20/2007 Last visit: 2/13/2024 Posts: 18 Rating: (0) |
Thank you very much Phantom your link was the exacly thing whichI seek for. Now I can consider my configuration. |
Follow us on