5/28/2020 8:06 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Berg, Can you right click the AS RT PO license of 1000 and check if it is not corrupted via Check option? Did you ever download the license from another ES? |
Last edited by: Oreca at: 05/28/2020 20:08:52If I could help you, you can use the RATE button. Thank you. |
|
5/29/2020 10:00 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Berg, Ok... I can provide two possible solutions: I see that you have installed PCS7 trial license. A restriction with trial mode is that the maximum capacity of OS objects is 250. Please remove/transfer the trial license and check if everything works. It's best if you restart the ES after removing/transferring the trial. If that does not work, I suggest you transfer the AS RT PO x1000 to a USB and then move it back to the system. After that, also do a restart to be sure. If that does not help, maybe something is going on with the project.. Maybe you can take a backup and see if the available licenses are listed in the PCS7 License information window... If that does not work, I suggest you create a SR.... |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
9/3/2020 8:52 AM | |
Joined: 4/18/2017 Last visit: 3/29/2023 Posts: 7 Rating: (0) |
Hi! Berg, Did you fix problem? BR, Sergey V |
Follow us on