1/16/2012 4:22 PM | |
Posts: 2 Rating: (0) |
Maybe my questions are somehow very general. what i am trying to learn is how do i operate or monitor my program on the OS. |
1/17/2012 12:03 PM | |
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hi aiman,
sorry for late, yes...your question was a lil big general Here fast answers to your question: 1- yes, it's possible in different way, the better one (in my opinion) is make available the paramater of the CFC block you want monitor using the right attribute 2- it's no possible to use "array" in PCS7: each variable need "explicit declaration" (each variable need own unique name and had to be NOT in array). It possible to use array when don't need to shoe the data on the OS 3-the PCS7 manual installed with PCS7 "PCS7 - Programming Instruction for Blocks" explain how create "faceplate" related to "AS CFC block" (and block icon) but this manual it's not easy to undrstand; need a very good knoledge os PCS7 engineering Anyway, a good point to start should be the "PCS7 compendium - Part A" SIMATIC Process Control System PCS 7 Compendium Part A - Configuration Guidelines P.S.: search for chapter "Requirements for configuration in CFC" in this document, should explain why you got the error the block are outside the range hope can help a lil Regards |
This contribution was helpful to1 thankful Users |
1/17/2012 1:13 PM | |
Posts: 836 Rating: (100)
|
My predecessor gave the most answers. |
This contribution was helpful to4 thankful Users |
8/2/2013 10:26 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question was splitted to after compression and download my PLC is showing Internal Fault. Best regards O_Moderator |
Follow us on