Industry Online Support
Technical Forum
1/31/2012 1:45 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Make sure there you do not enable any additional components of Windows Server R2. See Add/Remove programs in control panel. Additional components found at http://technet.microsoft.com/en-us/library/cc785371(WS.10).aspx If using an intel network card, install the driver from pcs7 dvd Is message queing installed? like you did when you follow the installation procedure? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on