9/1/2021 8:21 AM | |
Posts: 198 Rating: (60) |
Hello, In this case, you can use the WinCC "License Analysis" tool (refer attached screenshot). The licenses with comment Ok are fine while the ones in red need to be addressed. In case you are using an ASIA version of WinCC (Chinese/ Micrex NX), this issue could arise because of the absence of a license dongle. From your pictures it is clear that you do not have any expired/invalid licenses in your Automation License Manager. Sometimes, this popup arises because of the same too. |
9/3/2021 11:06 PM | |
Joined: 8/19/2012 Last visit: 4/21/2024 Posts: 125 Rating: (0) |
Thank you for your reply. Please check the attachment the wincc analysis Best regards |
9/9/2021 6:27 AM | |
Posts: 198 Rating: (60) |
Hello, From your attached screenshot, this is what I could infer: You have exceeded the number of OS RT PO (OS Runtime Process Objects) which can be handled with your current available licenses. In addition to your current licenses, you need the count based 'OS RT PO' licenses which are available in the following counts : 100 or 1000 or 5000. Without the OS RT PO license, you will be able to view the runtime only for 2 hours and the editors like Graphic designer will only be available in demo mode. Ensure that you increase the number of licensed processed objects by installing additional appropriate OS RT PO license keys on the single station. You can refer this manual for the required licenses for different PCS7 configurations: |
Last edited by: Jen_Moderator at: 09/09/2021 10:25:56Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on