2/11/2015 9:36 AM | |
Posts: 56 Rating: (0) |
HIi Ok. Thanks for this. I am having some problem in the latest PCS7 Version. ie WinCC V7.3. We are having customized object. In the object there is one proery called alignment left and right. In this version the text field is showing empty.In the older version its working fine. As well as there is pie Segment in the standard object it is also there is a small mismatch in the angle of 90 x 90. Please help me on this issue. Here I have attached the screenshot also.
------------- |
Last edited by: Min_Moderator at: 2/11/2015 10:35:56 AMNew subject after splitting |
|
2/11/2015 11:39 AM | |
Posts: 56 Rating: (0) |
Hi Here I have attached the version screen shot for your reference. |
2/11/2015 12:52 PM | |
Joined: 3/24/2009 Last visit: 8/7/2023 Posts: 406 Rating: (3) |
Hi, Can u tell me what are all the objects u have combined as a customized object? |
All is well :-) |
|
2/12/2015 6:17 AM | |
Posts: 56 Rating: (0) |
Hi Two IO filed and one button in the customized object. |
Follow us on