9/28/2017 2:30 PM | |
Posts: 34 Rating: (0) |
Did someone check this post ? |
9/29/2017 7:25 PM | |
Joined: 6/23/2008 Last visit: 4/22/2024 Posts: 1165 Rating: (279)
|
Hello Amen Allah, the quantity of '1' for the license package for 'PCS7 OS SW SERVER REDUNDANCY' is correct because it contains the licenses for one pair of servers. The licenses of this package need to be distributed to both server. So you can add a cross for this row also at 'SERV2' Do you have a redunant AS? You need the license 'HARDNET-IE S7 REDCONNECT PP V13' only if have redundant AS in your project. Are you aware that you won't be able to edit everything on your 2nd ES if you don't purchase licenses for the addons (Logic Matrix Tool, S7 F-Systems etc.) for that 2nd ES, too ? I'm not sure, but is it not like that, that the license for the 'PCS7 LOCIC MATRIX VIEWER' belongs on a Operator Station instead of the ES? I mean the same principle like for the 'SAFETY MATRIX VIEWER'. The rest looks good for me. Btw... I don't agree with the statemant from Myst below:
Of course you can dowload also from 2nd ES. Maybe Myst recommended this because of the issue like in this thread (see only the new question directly before my answer in that thread) ? Best regards... |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
10/3/2017 7:17 PM | |
Joined: 6/23/2008 Last visit: 4/22/2024 Posts: 1165 Rating: (279)
|
Hello Amen Allah, if your ES is connected to the network and the real OS servers are running, clients maybe connect wrongly to the ES instead of a server. Also problems regarding data synchronization could occour. Also you should know that you are creating runtime data in the ES project. When downloading the project to the server(s) problems like the one from this FAQ could occour (see 'Possible cause 1...'). Also this FAQ gives a few information about this question. Honestly said, I feel anoyed of always starting the os simulation during working offline. I mean as long as I'm working in the office on a project (without running real servers in the network), I often start the runtime on the ES (not by OS simulation). But after doing this, before downloading the project to a real OS server on site, I perform the relevant steps, from this FAQ. Best regards... |
Last edited by: mark1507 at: 10/3/2017 7:33:49 PM"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
This contribution was helpful to1 thankful Users |
10/4/2017 11:47 AM | |
Posts: 34 Rating: (0) |
I'm very grateful to your support mark1507. Thank you so much |
This contribution was helpful to1 thankful Users |
Follow us on