4/16/2015 9:23 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Dear Experts, I have installed PCS7 V8.0 SP1 on my laptop with Windows 7 as an OS. i am facing problem with WinCC, when I create new project in winCC or add OS station in PCS7 project, I am not able to create it, if LAN is not connected.I get error "Unspecified Error" and Project get closed. If I connect LAN connection and try, then everything works fine. How to resolve it? Please suggest. By connecting LAN , does any service starts which is necessary for creation of WinCC project? Warm regards, Damayanti Bhapkar -------------- |
Last edited by: CS Moderator at: 4/16/2015 1:16:33 PMnew subject after splitting |
|
4/19/2015 7:42 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Dear, I tried by assigning valid IP address, still problem not resolved. Anything else can we try? Damayanti |
4/20/2015 8:53 AM | |
Posts: 567 Rating: (106) |
Hi Damayanti,
thanks for feedback. I know the issue and I have solved it with a valid IP. So there must be another reason for the issue . Maybe there some other settings not correct. Did you check your network settings? They should be as described in PCS 7 Compendium Part A chapter 3.3.5. Link: https://support.industry.siemens.com/cs/ww/en/view/107196780/72204301323 Especially the hints are very usefully. |
Follow us on