11/17/2015 12:48 PM | |
Joined: 5/9/2015 Last visit: 2/5/2024 Posts: 81 Rating: (4) |
Hello, I have the same issue. i am using PCS7 V8.1 and S7-PLCSIM V5.4+SP5+Upd1. I have tried to download the Hardware configuration only, but still getting the same error while downloading Net pro connection. Attached pls find the error message. Please advise the solution. Best regards, Naresh Saini ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/18/2015 11:06:41 AMNew subject after splitting |
|
11/18/2015 11:25 AM | |
Posts: 567 Rating: (106) |
Hi, did you configure the PC-Station and did you set the correct PG/PC-Interface? |
4/27/2016 1:55 AM | |
Posts: 45 Rating: (0) |
Hello, I have the same problem here !!! |
4/27/2016 12:40 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hello, Which interface is used for the plant bus connection? If it is the integrated PN/IO interface of the CPU410 (X5 or X8), only TCP/IP protocol is available, not ISO protocol. PLCSim will set the correct PG/PC interface for you. You can leave the PG/PC interface to recommended: "PC_Internal". |
If I could help you, you can use the RATE button. Thank you. |
|
4/29/2016 5:27 PM | |
Posts: 45 Rating: (0) |
Hello, I'm sorry but I did'nt understand ur solution. |
Follow us on