7/9/2020 8:50 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, The option: "With reorganization (slow)" will check the S7 data storage as well. The system will check projects and libraries and reorganize them as well and in result, it may reduce the memory needed. Be sure that you need to have installed all software packages to execute that option, otherwise it will fail. See more info below:
See the following link what you must watch out for when using this option: Link The option: "With backwards compatibility" is a newer option in PCS7, but I don't think you will ever need this option in PCS7. This option will let you open the project with an earlier version of step7. Since step 7 is integrated in PCS7, this makes no sense. |
Last edited by: Oreca at: 07/09/2020 20:56:03Last edited by: Oreca at: 07/09/2020 21:08:43If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
7/10/2020 8:04 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi goodmorning, Hmm, I thought you meant "With backwards compatibility", because in my V9.0 I don't have this option: Download compatible. When in the Save as dialog, press F1 and you will be able to see information on it.. |
Last edited by: Oreca at: 07/10/2020 08:05:38If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
7/10/2020 9:25 AM | |
Posts: 66 Rating: (0) |
Hi Goodmorning! Please be informed today have tried by checking with F1 could not find the information related to OPTION --> with download compatible. Thanks |
7/10/2020 11:24 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, Thx for the feedback. Maybe Siemens renamed it... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on