11/16/2020 10:23 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi ABCGGKK,
In PCS 7 you can configure the size of the "Alarm Logging". The Alarm Logging ist the archive for all messages. The maximum size of a message is 4 KB, so if you want to archive minimum 10.000 messages the size of the Alarm Logging has to be at least 40 MB. For more information see the manual PCS 7 Operator Station at section Determining the archive storage capacity requirements.
In PCS 7 it is also possible to get the time stamp with a resolution of 10 ms. For more information see the manual PCS 7 High-precision time stamping With regards |
This contribution was helpful to2 thankful Users |
Follow us on