1/17/2020 8:28 AM | |
Joined: 8/1/2019 Last visit: 5/13/2024 Posts: 299 Rating: (3) |
Why are some foldes in plant hierarchy are green? |
1/17/2020 8:57 AM | |
Joined: 8/1/2019 Last visit: 5/13/2024 Posts: 299 Rating: (3) |
I didnt understand what you mean. |
1/17/2020 10:34 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Me neither, but it means that those folders are listed as batch category. So, if you are using batch, you can define which level is process cell, unit level, equipment module level or equipment phase. So if you are not using batch, it's no point of using. When you right click the foldername, you can go to tab: S88 Type Definition. In there you can select the level. The levels are set according to ISA88. When you have defined a level as process cell, the next level to be used is unit and so on. You can create neutral folders between, but all comes to play when using batch. |
Last edited by: Oreca at: 01/17/2020 10:39:12If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to4 thankful Users |
Follow us on