6/26/2020 3:57 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear nikola_hadjinikolov, yes, that data might affect your result. There is one possibility that i could think of, your block version is wrong or you did not install the library and use the latest block. To check/fix it, 1. open up the block properties of PCS7AnIn, check the version of the block. If it is the latest one, then maybe you have other types of issue. you may also update your libraries to the current version and try again 5. Library. 2. If the block version is wrong, please go to Simatic manager - > open-> library-> select PCS 7 V9 library -> look for your block in the block folder -> copy and paste in your master data library and your block folder 3. go to your cfc editor->option->block type-> select the blocks that you imported-> press the "->" from block folder to chart folder -> update- >yes. Done. Try to compile with generate module driver, and see whether the issue resolved. Hope this is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
6/29/2020 2:25 PM | |
Joined: 3/13/2015 Last visit: 4/22/2024 Posts: 122 Rating: (38) |
If the block update did not do the trick. Some remarks:
A work around to get the value out is to put de input DataXchg1 to 16#4 |
Last edited by: Molthoff at: 06/29/2020 14:26:07 |
|
This contribution was helpful to2 thankful Users |
6/30/2020 2:45 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Nikola, Thanks for posting your resolution here. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on