5/10/2019 4:39 PM | |
Joined: 10/5/2016 Last visit: 3/11/2024 Posts: 84 Rating: (0) |
Dear guys, I am modifying a fully working ES/OS Client and OS server PCS7 v6.1 project. I wanted to add some screens to the existing one which is working .I am having problems only with the TAGS (newly created) I am using the AS-OS compilation and S7_m_c attribute @ (variables inside db ,db>properties and db>special object properties ) to create tags automatically in wincc tag management. Allexisting wincc variables are directly connected to DBand not from any block from PCS7 library (i.e digimon or meas_mon), hence i am following the same. When i create a new db and variable with S7_m_c attribute and compile , i am getting the variable inside the tag management editor but when i connect to a io field it is greyed out. I tried to evaluate the tag status of the variable, and got"Tag not Found" What may be the reason ,i am gettingtag not foundstatus of the variable.. Only thenewly added variables in the dbare having this problem..existing variables i am able to monitor. How to rectify this?? Kindly find attached screenshots for reference.. AttachmentPCS7 tag error (1).docx (23 Downloads) |
5/10/2019 10:59 PM | |
Joined: 3/14/2008 Last visit: 3/18/2024 Posts: 2046 Rating: (922)
|
Hi, Did you also set attribute: "s7_m_c" for the DB block itself? Block folder->Right click DB->Object properties->go to tab Attributes and enter s7_m_c. |
If I could help you, you can use the RATE button. Thank you. |
|
5/11/2019 8:19 AM | |
Joined: 3/14/2008 Last visit: 3/18/2024 Posts: 2046 Rating: (922)
|
Hi, Ok , this was not clear to me in your text. How did you connect the IO field ? Can you show me a print screen. Are other signals working fine in runtime? |
If I could help you, you can use the RATE button. Thank you. |
|
5/12/2019 8:48 AM | |
Joined: 10/5/2016 Last visit: 3/11/2024 Posts: 84 Rating: (0) |
Hi Oreca, The other tags are working in runtime..Attached screenshot for io field config of newly created tags.. Clients: OS1- OS5 (5 NOS) Server A and B (Redundant).. Engineering station-1 no But now only one client (OS2) is working which is located in another place,all other clients are removed. These are the systems connected to Terminal bus now," ES1,OS2,SERVER A,SERVER B" Now runtime is in engineering station runnning from "OS3" project...I have Downloaded and compiled changes to os server (i.e adding screens), which is reflected in the client. Also manually updated server data in client project.. AttachmentIO field.docx (31 Downloads) |
Last edited by: arunvt1992 at: 05/12/2019 08:50:42Last edited by: arunvt1992 at: 05/12/2019 08:52:01 |
|
Follow us on