5/21/2013 1:07 PM | |
Posts: 24 Rating: (0) |
Hi Guys, I just want to know if step7v5.5 sp2 is compatible with pcs7v7.1 sp2 or sp3 ! I already check the siemens compatibility tool but it only shows step7v5.5 without any service pack. But i have download the compatible list for pcs7v7.1 and same is attached herein attachment, it shows step7v5.5 upd5 is compatible. i can not understand what is update5 ? I have created one S7-300 plc project in step7v5.5 sp2 and same i have to integrate in multiproject in pcs7v7.1 in which step7v5.5sp1 is installed. so i am bit confused about installation of step7v5.5sp2 on engineering station. Looking forward to find the solution. AttachmentPCS-7_V7.1_compatibility-list_en_2013-04-15.zip (40 Downloads) |
5/21/2013 11:39 PM | |
Posts: 24 Rating: (0) |
Thanks Mark for your valuable information. Best Regards Ashish Singh
|
Follow us on