6/22/2011 2:00 PM | |
Posts: 3 Rating: (0) |
Dear Friends We’re going to implement the attached configuration and use PDM station to perform setting and calibration of field transmitters. As I know, first, we should import the “.ddl” file of each transmitter into PDM using “PDM manage device catalog”. I have downloaded the device package including “.ddl” file from SIEMENS web site. But when I want import it to PDM library, the following error appears: “COMPILE ERROR while processing line : c:\siemens\pdm\sim_pdm\devices\hart\SIHASTIDENT02.inc(8): include file (Manufacturer_List.h) cannot be opened” What’s the problem?! The attached docs show the details. Sincerely javid AttachmentPDM Config_Error.pdf (58 Downloads) |
6/28/2011 3:38 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Seems the installation of it isn't completed or isn't correct. Repeate it again. Best regards, Hristo MIhalev |
6/28/2011 3:41 PM | |
Posts: 41 Rating: (4) |
Hello Javid, If you use the SIMATIC PDM as a stand alone tool (without integration in Step 7, PCS 7)then download the version SIMATIC PDM V6.0+SP5 and device library (contains Sitrans TW device description). For this version you can use your existing licenses. http://support.automation.siemens.com/WW/view/en/35125986 or contact the Service&Support (Support Request) to get the device discription for your PDM version. greetings |
Follow us on