8/7/2019 8:15 AM | |
Joined: 7/9/2015 Last visit: 3/28/2024 Posts: 3801 Rating: (553)
|
Hi, what you mean is S7-Routing. Please check the following FAQs: First check if your modules / PLC supports this function: Which modules support the "S7 Routing" function in S7 subnets?Then check the next FAQ. There you get informations how to edit this in NetPro What requirements must be fulfilled and what should I watch out for when executing Routing?Regards,Towome |
|
|
8/28/2019 1:14 PM | |
Joined: 5/3/2017 Last visit: 2/2/2024 Posts: 673 Rating: (216) |
Hello Soroosh.v, you can find the requirements and a lot of information about PDM in the Delivery release: SIMATIC PDM V9.1. For example, the compatibility with PCS 7: "SIMATIC PDM system integrated (in SIMATIC PCS 7/STEP 7) The statements regarding the migration and update of SIMATIC PCS 7 apply for applications of SIMATIC PDM integrated in SIMATIC PCS 7. In principle, it is possible to use SIMATIC PDM V9.1 from SIMATIC PCS 7 V8.2.x without limitations (except for FF option)." With regrads |
Follow us on