6/22/2010 1:22 PM | |
Posts: 30 Rating: (0) |
Can someone provide me a link to download the PDM free with 1 tags or maibe more or without tags. I am new on this software. |
6/22/2010 1:41 PM | |
Joined: 1/17/2007 Last visit: 3/8/2024 Posts: 1541 Rating: (531)
|
PDM is not free. There is, however, a free demo version that runs for 60 days. Here are the details. If you are asking for a hacked / cracked version, you will not find it here. |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
6/22/2010 2:29 PM | |
Posts: 30 Rating: (0) |
Where is the demo version...? Tomorow I will start again... |
6/23/2010 12:08 AM | |
Posts: 2661 Rating: (279)
|
See the following link:SIMATIC PDM 5.1 + SP2 Download |
This contribution was helpful to3 thankful Users |
6/24/2010 9:02 AM | |
Posts: 30 Rating: (0) |
Thank you Phantom75... A good year! |
4/8/2013 5:49 PM | |
Posts: 7 Rating: (0) |
Phantom, is this software still available? |
4/8/2013 6:02 PM | |||
Joined: 9/27/2006 Last visit: 4/20/2024 Posts: 12256 Rating: (2664) |
Hello J.Lash; Here is a link to the version 8.0 demo version of PDM:
Product Package for the use in a SIMATIC S7 / PCS 7 Configuration Environment with the following functional restrictions • Save Function disabled • Export/Import Function disabled • Expanded Functionality disabled • Communication Functions usable on a restricted Basis In 5 languages (English, German, French, Italian, Spanish); Software Class A; executes under Windows XP Professional 32-Bit, Windows 7 Ultimate 32-/64-Bit, Windows Server 2003 R2 Standard 32-Bit or Windows Server 2008 R2 Standard 64-Bit; Hope this helps, Daniel Chartier |
||
4/8/2013 6:55 PM | |
Posts: 7 Rating: (0) |
this appears to be a non communicating DVD demo version.. I am needing a demo version that i can install and dive into a device with. |
4/16/2013 10:36 AM | |
Posts: 836 Rating: (99)
|
Hi, check out this page on the Siemens Industry Mall for details about he PDM versions. Either you can use PDM V6.1 Single Point where you can connect to one device, or you can use PDM V6.1 Basic with a minimum of 4 Tags. If you like to use PDM V8.0 you either have to use it with PCS 7or Step7. So if you like to use real communication you have to buy some version with the smallest ammount of tags. Another good idea would be to contact the regional contact of siemens which you can find over this link. |
Follow us on