7/18/2019 10:28 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
what kinds of simulation? PLC Sim? Simit? any sample screenshots? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/3/2019 7:53 AM | |
Joined: 7/27/2016 Last visit: 3/25/2024 Posts: 50 Rating: (0) |
Dear simulation mean when we put Analog value to simulation to force some value... |
8/3/2019 12:30 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear HAMEE, to simulate a value, there are multiple ways. 1. You can simulate values by using APL Function Blocks from HMI, 2. You can simulate values using Pcs7AnIn channel driver blocks 3. you can use "Forcing" to turn input to force mode and force a simulated value in CFC function blocks. 4. you can use "SIMIT" to send value to signals /hardware IO to the function blocks. (my method) So, it will be better if you attached some screenshots or trending. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/8/2019 1:28 PM | |
Joined: 7/27/2016 Last visit: 3/25/2024 Posts: 50 Rating: (0) |
Dear Rahaei, Can you please describe in detail?? |
Last edited by: HAMEEE at: 08/08/2019 13:29:07 |
|
8/9/2019 9:16 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello HAMEE, as described by JazTai there are serval ways to simulate an value. One way is to use the input SimOn by the channel blocks (meant by Rahaei). With an "1" at the SimOn the PV_Out is the value at the input "SimPV_In" and not the input "PV_In". More information about simulation signals you can find in the manual PCS 7 Advanced Process Library at section Simulating signals. With regards |
Last edited by: Heisenberg2 at: 08/09/2019 09:18:36Last edited by: Heisenberg2 at: 08/09/2019 09:21:09 |
|
Follow us on